CMP#.REARM

Description

CMP#.REARM sets the automatic rearming behavior for the setpoint. It determines whether CMP#.ARM resets to 0 after a compare event, or stays set to 1 continuously. It may be changed while the compare channel is running and the setpoints are armed.

It takes two command line arguments: the first specifies the setpoint, and the second turns rearming on or off.

Examples

Usage

0: Disable rearming, enable single shot arming (default)

1: Enable rearming, enable continuous arming

2: Enable rearming, enable continuous arming and arms the setpoint on startup

Code

The first two commands turn on rearming for setpoint 0 of channel 1, and turn off rearming for setpoint 4 of channel 2. The last two commands turn on rearming for setpoint 4 of channel 2 and automatically arms setpoint 4 of channel 2. The setpoint will remain armed on startup if DRV.NVSAVE is performed.

--> CMP1.ARM 0 1
--> CMP2.ARM 4 0 --> CMP2.REARM 4 2 --> CMP2.ARM 4 --> 1

Context

See Compare Engines View.

Versions

Action Version Notes
Implemented 02-06-00-000  

General Information

Type

Read/Write

Units

N/A

Range

0 to 1

Default Value

0

Data Type

Integer

See Also

CMP#.ARM

Stored in Non-Volatile Memory

Yes

Variants Supported

All variants are supported.

EtherNet/IP

ID

Instance

Attribute

Name

Data Type

Access

User Mappable

31340

1

31340 (0x7a6c)

CMP1.REARM

Unsigned8[8]

Read/Write

Yes

31341

1

31341 (0x7a6d)

CMP2.REARM

Unsigned8[8]

Read/Write

Yes

PROFINET

Parameter

PNU

Data Type

Access

Units

CMP1.REARM

31340

Unsigned8[8]

Read/Write

-

CMP2.REARM

31341

Unsigned8[8]

Read/Write

-